Hello,
I've attached a image of the current PMU setupusing the tps65721 to generate 3.3V on the DCDC converter and then produce 1.8V on the LDO and I just wanted to verify that my design looks ok. In addition, there is a mode pin that I currently left floating which determines whether the regulator is in PWM mode or PFM mode. Is it ok to leave that floating or should I tie it to gnd/VDD?
Thanks,
Sangeet