This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54386PWPR Inductors getting hot



We’re running our units and we noticed that the 2 inductors used in our TI dual power supply switcher (part # TPS54386PWPR) are running hot. We’re using the Wurth 74477110 and 74477112 for a +3.8V and +5V supplies respectively.

The +3.8 supply is powering a Cell Module Simcom SIM5320AD and the +5V supply is powering an LCD and is also feeding a 3.3V LDO that powers the rest of our board.


What we would like help with is why are the inductors getting hot? Should we use a different inductor?

  • The 74477110 should be ok-ish. it is rated for 5 A dT of 40 C. The 74477112 is only rated for 3.37 A. It is probably getting pretty hot. What is your input voltage and output currents? The values look a little low (the EVM uses 22uH). You can calculate the minimum recommended value. I wpuld probaly size the inductors for current at or above the current limit for each channel.
  • The input Voltage is 12VDC and +3.8Vout @ worst case 0.7A and +5V @ worst case 1A.

    Regards,

    Ed
  • Using the standard design equation for inductors:
    For 3.7 V output, if you design for the full rated output current of 3 A, then 4.7 uH. For 0.7 A, 22 uH.
    For 5 V output, if you design for the full rated output current of 3 A, then 4.7 uH. For 1 A, 18 uH.

    So those 10 and 12 uH inductors you chose are about midway. It just depends on how much ripple you want and how much of your load range you want to operate in DCM vs CCM.