This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to get two separate power supplies from one source?(plus what is a back to back diode?)

Other Parts Discussed in Thread: LM1086

Hello everyone.

In ADC application, I will need two separate supplies: +5VA and a +5VD , I use  two LM1086s to  achieve this, and the source is one same 24V.

I connect 24GND to AGND together(N108),  then I can't connect 24GND to DGND because I need +5VA and +5VD be separate(N109), will N109 work under this situation? What shall I do with this?

Next I want my AGND and DGND connected with a back-to-back, is this the right back-to-back method?

  • The circuit for N109 will NOT work as the LM1086 GND pin, and the output load, need a current return path back to the +24V input supply.

    " ... is this the right back-to-back method? ..."

    Depends on what you are trying to accomplish. As drawn, if AGND or DGND are more than about +/- 0.5V apart one of the diodes will conduct. So if your intent is to clamp the two pins so that the voltage difference between AGND and DGND does not exceed approx. +/-0.5V, this will work.

    If you need true galvanic isolation for '+5VD' you need to look at isolated ds-to-dc converters, or you will need separate (and isolated) 24V input supplies.

    www.ti.com/.../offline-and-isolated-dc-dc-controllers-and-converters-products.page