Hi Support,
Am trying to use this chip for my small solar panel and put a 870mAHr 1 Cell, 3.7V on the VBAT.
Would like to know the charging current from bq25570 like?
Reason: To try to charge the Li-ion at a safe Current limit.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Support,
Am trying to use this chip for my small solar panel and put a 870mAHr 1 Cell, 3.7V on the VBAT.
Would like to know the charging current from bq25570 like?
Reason: To try to charge the Li-ion at a safe Current limit.
Thanks.
Hi Support,
In addition, noticed the following when testing.
Attached a single cell Li-ion onto the VBAT, 8500mAHr
System Load is 1mA and my output set at 3V
When solar panel is under direct sunlight. My Output COUT will be 3V toggling On and Off at Load of 1 mA. BAT OK Signal will also be toggling High and Low
When I covered the solar Panel from sunlight . The output at COUT will be continuous Steady voltage at load of 1 mA.
I use the followings:
1) I follow exactly same value a written in yr datasheet
Page 24-25 Figure 24.
Except that output is set to 3V.. I have reverted back to 1.8V it seems like same problem
2). Solar Cells. I connect 2 in parallel ( See attached)
Thanks.
Hi ikon,
We charge by voltage and not current. It is analogous to CV charging. What is the charging current limit on your battery? With the 850mAH battery, we are under 0.3C at all times.
We are considering the current limit on a newer device.
thanks,
Gautham