I am considering using the TPS3808 reset pin in a non-conventional way and wonder if anyone has had experience with this idea, or who may want to steer me away from it for some reason. The design would use the open-drain reset line as a pull-down to short an ac waveform to ground. The signal is a nearly square wave at about 50kHz with a source impedance just above 10k Ohms. Two possible problems are 1. Pin capacitance may cause distortion to the signal when enabled. 2. Signal swing may cause unanticipated malfunctions inside the TPS3808.