Hi,
I am evaluating the SM72445 to include in a new design for one client and to replace some Linear Tech parts in some designs for another client.
I have a SM72445 EVM board and I have hooked it up to a solar panel simulator and and electronic load as per the evm user guide and it seems to work as expected.
I now need to test it with a 12 V sealed lead acid battery.
When I hook up the battery to the output with the simulator off, the battery voltage appears on the input. This should not be happening as far a I can tell.
Also when I run the simulator, the SM72445 only seems to only run in panel mode and not in MPP tracking mode.
Can I get some expedited help with this?
Thanks