Hi,
The recommended pad diameter for TPS63051 DSBGA is 0.23mm.
May I know 0.3mm diameter is still ok or not?
If so, that means the pad to pad clearance is only 0.1mm (0.4mm pitch - 0.3 pad diameter).
Is this 0.1mm clearance ok for 500mA application? (i.e. DRC check in EDA tool set to 0.1mm clearance)
Since for many PCB factory, the minimum BGA pad diameter capability is 0.3mm.
Thank you.
Regards
Rongfeng