This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Fast transient LDO: TPS7A7100 or the any other LDO

Guru 19645 points
Other Parts Discussed in Thread: TPS7A7100, TPS7A87, LP5912

Customer is considering TPS7A7100, but it was failed for FPGA's request transient.

Request spec is below.

【Request spec】

・Vin: 1.8V

・Vout: 1.0V

・Iout: 382mA_max

 Load transient: 61mA → 382mA at 1.4μs

         ⇒0.23A / μS

Is there proposed measure or the other matching LDO?

TPS7A7100 is modified below capasitor, but it didn't catch up transient spec.

・Cin: 10μF + 0.1μF

・Cout: 20μF + 0.1μF

Best regards,

Satoshi