The datasheet for BQ24195L (Revised December 2014) shows Bit 0 of REG05 (Charge Termination/Timer Control) as being reserved.
The GUI software (v1.5.0.1 along with the USB to I2C/GPIO dongle) for the EVM shows Bit 0 for this register as "Fast Charge Current at Low Temp" with a 0 being 50% and a 1 being 20%.
If the GUI is correct, is the "low" temperature related to thermistor "cold" temperature?
I am using a battery that I can charge at lower temperatures at 20% of normal charge and trying to figure out how if I can utilise this function to reduce the charge if the battery drops to a specific temperature.
Thanks