This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54232-EVM-415 Ic burning when used with external Lipo battery pack

Other Parts Discussed in Thread: TPS54232

I purchased 5 of this board TPS54232-EVM-415.

I intended to use this DC-DC regulator in my experimental set up.

My set up voltage is set to be at 16.8V and i will like the EVM board to regulate it to 12V and 2A output to support my system.

Testing of the board with a external power supply generator set at 16.8V and 2A input, the TI Dc-Dc board works perfectly.

However, when i changed the power supply to an external lipo battery pack providing 16.8V, 2200mah output, upon connecting the battery to the Vin of the board, a huge spark appeared and the IC chip on the TI board burnt.

May i know what is causing this issue?

I have tested the battery with 3 of my boards and all 3 suffered the same effects of having sparks before the ic chip burnt. All worked perfectly with the power supply however.

May i have some insight of why is this happening?

Thank you!