Hi,
on behalf of my customer I'm hoping you can help with a recommendation to solve the UCC28070 soft- and cold start problem.
- Problem 1: Delay during cold start some samples (25%) of the IC UCC28070 need more then 5s for cold start if the temperature is lower than -35°C
- Problem 2: Timing is not correct during cold start Converter starts at a very high soft start level and so produces an overvoltage at the output
Perhaps the two problems are due to the same reason
When the above problems occur, Fault or Restart should not be active because VSENSE, SS, VAO, UVLO and Temperature are in the correct range.
An extract and some timing plots are attached in a file.
Questions:Softstart and cold start problem of UCC28070.pdf
1. What is the reason for this behavior and what could be done?
2. Rsynth pin is very sensitive and it`s very easy to damage the IC via this pin. How is it possible to protect it without getting other problems?
Specification:
DC/DC Converter
Input 12…138Vdc
Output 125Vdc
Power 550…780W at the output of the two converters after the boost converter
Temperature range:
Minimum is -35°C …94°C outside and -35…+120°C at the IC
Best regards,
Uli