This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1H100 Protection Circuitry

Hello,

I'm writing for a detailed description of the MCU I/O Protection and GND protection.   In particular:

1. The datasheet suggests that we need 4.7kOhm for 3.3V I/O's and 10kOhm for 5V I/O's.     How are these resistances derived?    What are the calculations behind them?

2. TI recommends a parallel diode/resistor combination to protect the ground network.    Is this network only required is there is a potential for a negative voltage transient on GND?     The recommended components appear to be 1kOhm and a 200V/0.2A diode.    How are these values calculated?

Don