I have a question.
My customer are using LM5009.
LM5009 is used in the power supply for the control circuit of the fan motor.
Customer checked current at Vin pin.
Normal is a load current of about 10mA, but was flowing 1.2A peak to Vin pin to when to turn off the fan.
Customers are worried about whether the IC is broken.
Is this will no spec on the problem?
It is considering to circuit protection on the input side.
Best regards,