Hello TI:
I have a technical/application question on the TI TPS3808G01 Supervisory IC. We currently use this part on a OMAP-L138 based design as the main or master reset generating IC. We are experiencing a cold temperature boot problem of the L138 which is related to this IC. We believe we have found a solution to the problem, but were looking for confirmation the solution is ok as related to the application of the TPS3808G01. If so, below is a summary of the details.
Attached is a snippet of the Reset circuit. Note the TPS3808G01 Reset output pin is pulled-up to 3.3V with a 4.7k Ohm Resistor. The Resistor is located at the IC and is connected to 7 circuit loads across our PCB design.
As mentioned, we discovered a problem where the L138 would not boot at cold ambient temperatures below 0C. Upon investigating we discovered the Reset signal did not have a sharp low to high transition, but instead a slow stepped transition from low to high coming out of reset. We traced the problem down to a prior design change where an 8th load was added from a change to an L138 Boot Serial SPI Flash Memory IC with a Reset input. With some further investigation and testing we could eliminate the slow, stepped Reset signal, and the thus the cold temperature boot problem, with a change to the Resistor pull-up value to 1.5K Ohms from 4.7k.
In reviewing TPS3803G01 data sheet Page 4 Table and Page 8 Section 8.3.4, it mentions that the Reset output pull-up Resistor value should be no smaller than 10k Ohms. However, from what is spec’d in the data sheet, it appears 1.5k Ohm is ok since it does not exceed the 5mA absolute maximum Reset pin current noted on Page 5 Section 7.1 and Page 9 Figure 8.
Therefore, can you confirm a 1.5k Ohm pull-up Resistor can be used on the Reset output pin of the TPS3803G01 without any problems?
Any feedback or input is welcomed and appreciated!
Thanks again!
Paul