Dear all,
we would like to test the BQ76940EVM with actual batteries,
I couldn't find in the user guide explanation on what needs to be done.
I removed resistors R129-R138.
anything else? should I remove R122 too?
many thanks,
Ran
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear all,
we would like to test the BQ76940EVM with actual batteries,
I couldn't find in the user guide explanation on what needs to be done.
I removed resistors R129-R138.
anything else? should I remove R122 too?
many thanks,
Ran
thanks Willy,
so leave S3,S4 will solve it.
about order of connection.
in my actual schematics, I cannot physically guaranty the order of cell connection.
B- and B+ will be connected first, not sure what order, and then, V0-V6, followed by V7-V12 and V13-V14 (it is a 14S configuration).
what should I expect?
should I find a solution for this?
regards, Ran
Generally it should work fine, the part is designed for random cell connection. However 14 cells will provide a lot of voltage which could distributed across the inputs by the application circuitry or assembly tooling in a way to exceed the abs max ratings of the part. The chance of overstress may be less if the connectors match the groups on the IC (for 14 cells it might be V0-V5, V6-V10 and V11-V14). You might look at www.ti.com/lit/slua749, section 10. Connecting V6 might normally be a concern, but if you have already connected B- and B+ the power supply capacitors will already be charged. You may need to limit some voltages in a manner specific to your circuit construction and assembly process.
Dear Willy,
PCB is built (because of mechanical reasons) to accept:
randomly main B- and B+.
then harness with V0-V6 , V7-V12, V13-V14.
1) is connecting main B+ before B- a problem? should I make sure they are separated from V0 and V14 first?
2) from your explanation we expect no issue once B+ and B- are connected and then we connect the harnesses one by one.
because V6 is connected well after capacitors are full.
thanks, Ran