Other Parts Discussed in Thread: BQ25890, BQ24190
I have a small battery powered motor and motor controller application.
It uses a single cell Li/LiPo battery 5400 mAH. The device is charged by a USB charger/host, VBUS 5V, charge current 1.5A.
The VSYS is 4.2V and ISYS is 7 A for short 5-10 second durations, dropping to 500 mA nominally. The product does not operate when it is being charged - it only operates under battery power.
I am looking at the BQ24190 and BQ25890, but these devices show ISYS is limited to 4.5 or 5 A. What other devices are available with higher ISYS?