Hi ,
I am using 2 x UCC27611 to drive 16 Low voltage SRs with a total current of 97 mA, i noticed that the drop across the internal LDO is around 1V at this current, i.e the input voltage to the driver Vdd=5.4V and the reference voltage Vref=4.4V, this has around 0.1W is this the normal with this driver as the LDO currently consumes 20% of the total driving power i have.