This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54302 / Selection for inductance

Other Parts Discussed in Thread: TPS54302

Hi,

My customer is considering on following condition.

Vin : 5.0~20V, Vout : 5V, Iout : 3A

※ There is margin on the minimum value of Vin(5V) , the Vin doesn't drop until 5V actually.

I simulated on above condition by Webench, however it doesn't works and following message appears.

Is it difficult to design with TPS54302 on above condition?

Could you indicate if there is to pay attention when designing inductor value?

Best Regards,

Kuramochi

  • Kuramochi,

    The Webench can not support this kind of high duty simulation. That is because the their will be a voltage drop when the devices works in about 100% duty.

    Could you please descript the details of the application? how much the voltage drop can you accept? For this large duty and wide VIN application, you'd better apply

    one EVM board to check it.  

    Abull Yang