Hello all,
I am using TPS2544 for my application, which is to charge mobile devices in DCP mode from any USB power source. My application is specifically for Apple devices. So I set the IC in forced divider mode (CTL1, CTL2, CTL3 - 1,0,1). I observed that when an iPhone is connected the IC is in Divider 1 mode and it charges at 1 A approx, but when I connect iPad, the IC doesn't shift to Divider 2 mode and the iPad still takes only 1 A.
"TPS2544 will automatically switch between the Divider1 and Divider2 schemes based on charging current drawn by the connected device. Initially the device will set the data lines to Divider1 scheme. If charging current of >750mA is measured by the TPS2544 it switches to Divider2 scheme and test to see if the peripheral device will still charge at a high current. If it does then it stays in Divider2 scheme otherwise it will revert to Divider1 scheme" - (in datasheet)
Is there any version of the IC where I can set it specifically for iPhone and iPad DCP modes? I can not use Auto-Detect mode due to various reasons. Please help!
Thanks,
Pra