Hello,
My name is Crawford, I am working on a design for a client's wearable product that utilizes wireless charging. We have a prototype that uses the bq51013B but is not working. We modeled the design off the datasheet closely and I have attached a screenshot of our schematic. The nets "Coil+" and "Coil-" go to the antenna. "InductiveIn" goes to the battery charger we are using - another TI IC.
The antenna we are using has a 9.5 mm circular diameter. This antenna can be seen here: https://www.digikey.com/product-detail/en/abracon-llc/AWCCA-12R12H11-C01-B/535-13306-ND/5801533
We have been testing with a Qi compatible transmitter, but it seems like the transmitter is attempting to communicate with the receiver, but is never receiving the signal to start providing power. Approximately every 5 seconds we see a sinusoidal pulse on each end of the coil. For the remainder of the time, Coil+ and Coil- are effectively ground. A screenshot of the input on on Coil+ is also attached.
We are hoping to gather some input as to why we are having issues with the inductive receiver. Any input is greatly appreciated.