This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27421 average current



I'm having an issue measuring average current with the BQ27421 gas gauge IC.  It will sometimes give the correct value (8-10mA for my system), but for long stretches it will output 0mA, which is obviously incorrect.  Sometimes it will randomly jump back to the correct values after a little bit, other times I need to reset the device.  
I thought the IC automatically entering sleep mode might have been the cause so I disabled sleep mode in the OpConfig register, but that had no effect.  Reading battery voltage and state of charge always give the right values, so I know I'm talking to the IC correctly.  
Has anyone seen this before, and is there a fix? 
Thanks,
Ben