This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28600 Method ON/OFF from the outside(Enable function)

Other Parts Discussed in Thread: UCC28600

UCC28600 Team,

 

Many thanks.

 

We received a question about I/F which let UCC28600 circuit have ON/OFF from the outside(external signal).

 

Could you please tell me the method concrete.

 

 

Best regards

___________________________________________

Katsunori HAYASHI

Engineering Professional

FAE Group/Metropolitan Area/Sales_&_Marketing

Texas Instruments Japan Limited. (TIJ)

TEL:+81-3-4331-7120         E-mail:k-hayashi@ti.com

  • Hayashi-san,

    It should be possible to interface an external remote on/off signal to the UCC28600 SS (soft-start) pin.

    If this pin is pulled low, the PWM will be disabled, and will remain disabled as long as SS < 0.8 V.

    Depending on the logic polarity of the external on/off signal, the interface to the SS pin may be different. The SS pin can be pulled to GND by and open-collector npn, or open-drain nfet, or through a pull-down diode. Since there is an internal offset on the SS pin of 1 V (0.8 V min), it does not need to pulled all the way to GND, so a pull-down diode may be used.

    I hope this helps answer your question.

    Thanks,
    Bernard
  • Bernard-san,

     

    Many thanks.

    I received your reply, and so thanks.

     

    Best regards

    ------------------------------------------------------------------------

    Katsunori HAYASHI

    Engineering  Professional / Power  Management

    Field  Application & Solutions / Sales  & Applications

    Texas  Instruments  Japan  Limited. (TIJ)

    TEL:+81-3-4331-3689          E-mail:k-hayashi@ti.com

    ------------------------------------------------------------------------