Hi, sukumar here from bangalore.
Actually we are facing the problem in TPS5450 output short-circuit protection. We are using connector at the output end and we are performing short after the mated connector(may be 10cm away). So when we short it is drawing 7A current output side continuously and 0.7A input side. And we observed vsense is not going to ZERO voltage since 150mV is coming output side.
Can you please suggest any solutions to make vsense to "ZERO" voltage.