Hello there,
I have a problem with the temperature calibration of the BQ40z50-R1
“Calibration – Calculated external sensor two temperature correction is out of range” ( Sometimes the error also shows as sensor one)
Has anyone got an idea of what could be wrong here?
In my application I have the following parameters:
* Battery voltage (VBAT) -> typ. 14,6 V, max. 16,8V
* Input current (IIN) and voltage (VBUS) -> VBUS = 3V3
* System voltage (VSYS) and current (ISYS) -> IDSG = 2750mA
* Charge current (ICHG) -> 1375 mA
* Registers setup (I can share the relevant parts if it is required)