Hello,
During RTCA/DO-160E, Section 20 Radio Frequency Susceptibility, Radiated Susceptibility, the unit experienced failures between 230 and 400 MHz during the 0.1-1GHz CWSW 100V/m (category W)]. We isolated the failure to the TPS62140 circuit.
In our application, Vin=13.5V Vout=3.3V Per Figure 7 in datasheet FSW=Low, L1=2.2uH, Cout=10uF, Cs=4.7nF, instead of Cin=10uF there is a pi filter 10uF, 2.2uH and 47uF which is connected to PVIN and EN pins. There is an additional filter stage 10uF, 100ohm, 0.1uF before the AVIN pin.
Question: Throughout datasheet recommendation is to tie AVIN and PVIN together. What are the differences between the AVIN and PVIN pins? With the RF voltage on 13.5V input, the voltage at PVIN pins may be different than the voltage at AVIN pin, what is the effect of this difference?