We are observing that the Band(High/Low) is not changing on the LNB monitor, even after the LNB is configured according to the datasheet.
The LNB is configured by setting bit 3 (EN) of Control Register 2 to 1 and then setting the bits VSET0 to VSET3 according to table 6 to get voltages of 13.4,14,18.2,19.4 and 20 (any one voltage at a time). These settings are done using the I2C interface. But there is no change in the LNB voltage output – it remains greater than 15V as seen on an LNB monitor. Is there any sample code which illustrates how to set the output voltage?
Also, how is polarization changed from vertical to horizontal and vice versa?