Other Parts Discussed in Thread: UCC27211A-Q1, CSD19536KCS
Hello TI,
I got a circuit based on the Fig. 18 (Page 11 UCC27211A-Q1) (VDD: 12V HB bypaa capacitor 100 nF) . I want to switch 100V (as in Application Diagram) wit 6.7 kHz. The problem: As soon as the high-side FET is active the voltage on HS should increases to 100V but the UVLO (Undervoltage Lockout) disables the high-side driver (as written in chapter 8.3.2) when reaching VHB UVLO threshold. This produces a ringing of HO within the UVLO Hysteresis
Question is how to prevent this behavior?
I want a constant 100V rise/hold on HS as long as HI (so should HO) is aktive.
Thank you very much for support!