This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8758-E0 Max duty

Other Parts Discussed in Thread: LP8758-E0

Could you let me know the LP8758-E0 Max duty value?
We would like to judge the output voltage upper limit.

Best Regards,
Kohei Sasaki

  • Hi Sasaki,

    Duty cycle of the LP8758-E0 is not limited. It can go up to 100% if input voltage = output voltage.

    This is not correct. There is definitely a 0.7V drop out and the PWM duty cycle does not go to 100%. It is however capable of 4A load 100% of the time if the heat sink is designed properly, but this is not the same thing.
      Set your input to >3.7V to remain in regulation.