This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS73101 unstable at 5.2 to 5@100mA

Other Parts Discussed in Thread: TPS731

Hi All,

I'm hearing about some stability issues with the TPS73101.

The system set up:

  • Input = 5.2
  • Output = 5V
  • Current = < 100mA
  • "Had to put a 1Ohm resistor in series to stabilize the device to achieve the desired 45 deg phase margin"

They do not want to have to use the resistor to maintain stability.  Is this the expected behavior?

Regards,

Aaron