We've developed a custom cape for use with the BeagleBone Black Rev C. The cape supplies 5V to the BBB at Pin 3 of J9 which goes to the AC input of the BBB. The cape is connected to a 12V supply and features a supercapacitor backup supply when 12V is removed. Once the supercapacitor voltage drops to around 4.3V, the BBB shuts off. If 12V power is reapplied, the power does not come back on unless the capacitor voltage (AC) drops to below 3.3V. Is this normal functionality of the TPS65217?
Thanks,
Travis