Hi,
I have designed a TPS7A33 test board according to the layout and recommendations of the datasheet but after soldering the output of the regulator was not regulated. It's valuable to say that at first I have set Css/nr to 1uF. In this case the output descent from desired voltage to about 0V in about 1 minute. When I changed this capacitor to 10nF, the outputs follows the input voltage and after a while the output jumped to zero and now it is always zero even after turning input on and off.
I have used the vqfn package. I have soldered two different boards but none of them work correctly. After this I have checked another IC. The thermal pad is not connected internally to the GND of IC but in the datasheet, it is indicated that it is connected internally to the ground. Anyway, in my layout, thermal pad is connected to a large GND plane. Below you can fine the layout. Please help me!