This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ20Z95, Lifetime data update period

I am looking for an explanation of when the BQ20Z95's lifetime data. 

Using the 'bq Gas Guage' application I have configured various lifetime parameters e.g. max temperature is set to +10 degC. I have confirmed these values by reading back from the PRO page and the DATA FLASH page. My problem is that the lifetime values never seem to change. I can see that the pack temperature as read from the SBS page is at +21 degC, but the lifetime data has not changed.

  • When does the BQ20Z95 actually update its lifetime data?
  • Various posts talk about a 10 hour period for these to be written. Is this only when written to flash? 
  • Is there a RAM copy of the data?

  • OK, it looks like I needed to perform a device reset (Manufacturer Access: 0x00, Reset: 0x0041).

    After I have done this the device is now updating the lifetime values as expected.

    So another question:

    • How should I have known that a RESET was necessary? Is this flagged somewhere?