This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to determine the result of the Calibration for BQ20Z95 while in Calibration Mode?



Hi TI Support,

I'm working on developing an automated test system for our batteries. We use the BQ20Z95. We've discovered that the temperature reading returned from the battery is not a good indication of whether the thermistor hardware is good because it will return the highest value of the three temperature sensors (int, ext1, ext2). It seems as though a defect can be present that is either ignored or returns a value much too low so it is not reported.

When I calibrate the defective battery in question using the TI evaluation software I receive an error message (5026) which indicates an overflow occurred with a Temp Sensor. When I manually perform calibration through the TI software by sending each byte individually it seems to work.

The process I use is the following:

Set Calibration Mode: send 0x00 0x0040

Write the actual temperature: send 0x62 0x0B99

Start calibration: send 0x51 0xC038

Read back 0x52

0x52 will return 0xC000 which would seem to indicate calibration completed.

I'm unable to read the Battery Status register while in calibration mode so I can't determine the results which I assume would be reported from bits EC3, EC2, EC1, EC0.

After I send 0x73 to get out of calibration mode (I'm not storing the calibration results - there's no difference if I do though) the battery status register returns 0's for bits 0, 1, 2, and 3.

So how do I detect when a calibration fails??

Thanks!

Matt