Hi, all.
I try to estimate the junction temperature of TPS62180 by following condition.
12Vin 3.3Vout 6A Efficiency=90% Ta=25C
When loss is estimated at 1.72W and θ ja is calculated by 61.5 ℃/W, the junction temperature closes beyond 125 ℃.
But I think that it doesn't become such high temperature in EVM.
Is the value of θ ja right?
Best Regards,