Customer is evaluating TPS65235EVM, but below problem is occured.
Please let me know about proposed measures for three points below.
-----------------------------------------------------------------------
①Sound noise is occuring, customer spec is below.
・12Vin→11V~15V / 600mA_max
・Sound noise is only 11Vout, 15Vout is no problem.
・When 11Vout;
No load→No sound noise,
Light load→Occure sound noise. If increase current, sound is high key.
More than 400mA→No sound noise
②Therefore EXTM pin input 44kHz(3.3V), sometimes clock output is 22kHz.
Is there way to certainly 44kHz output?
③otherwise, if below pin unused, are these pin left Open OK?
#14:DOUT, #15:DIN, #19:GDR
-----------------------------------------------------------------------
Best regards,
Satoshi