Hi team,
My customer use the TPS564201 to replace the TPS54428.
But the TPS564201 output ripple is not good as the TPS54428.
Please refer the attached test report.
Is there any comment to improve the output ripple?
thanks.
Prescott
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Prescott,
As aligned in the email,
The ripple of load transient is out of customer’s requirement;
For 0A to 2A, 1A to 3A, 2A to 4A, our test results is reasonable;
We’re using the right method to test the ripple;
Action item:
Check load transient 0A to 4A – Nick