I want to use the UCC29950 device for PFC control only. Input is 115vac, and eventual output will be 36v at 50amps. lOAD variation is 100% to zero. This is for supply for a 50amp battery charger.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Peter-san,
Could you tell me about UCC29950?
My customers are interested in this device.
Does this device is using UCC28180?
Customers are using the UCC28180.
For that reason,
They are expecting that has a built-in familiar device(UCC28180).
Please the detail information of combo chip.
Best regards,
Yusuke/Japan Disty