Hi
One of my customer want to use RF LDO LP5907 for camera sensor power. They need 2.9V output from 3.3V.
3.3V is comming from DC to DC module.
As per data sheet VDO = 250mV(Max.) @ 250mA for X2SON package. Also datasheet is showing VIN = VOUT(NOM) + 1 V & recommending VIN voltage must be at least VOUT + 1 V.
Customer requirement is 2.9V out of 3.3V, will this work reliably or do they need to consider the input as 3.9V?
To reduce the output noise of LDO any further recommaendation also helps. At present we have suggsted them to keep provison for ferrite bead at the output to prevent switching noise or any other RF noise to CMOS sensor.
regards,
Mitesh