This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How TPS5450 can be used for 19V 3A application

Other Parts Discussed in Thread: TPS5450, TPS54561

I am using TPS5450 for 19V output with 3A load current. I have calculated the inductor value accordingly which comes around 1uH. Iam using shielded inductor from coilcraft. I have calculated the feed back resistors value according to the formula R2 = R1 * 1.221/ (Vout - 1.221) to set the output voltage to 19V.

Problem : When the input voltage is increased till 10 volt the output raises upto 6.7V and then it decreases when the input voltage is further increased to 25V.

My requirement is as follows :

1)Input voltage  - 22.4V to 29.4V 

 Output voltage - 19.5V Output current - 3A

2)Input voltage  - 22.4V to 29.4V 

 Output voltage - 19.5V Output current - 4.6A

3)Input voltage  - 22.4V to 29.4V 

 Output voltage - 19.5V Output current - 4.6A

Kindly help to to design proper circuit using TPS5450