Hi
My customer did not find the Thermal Information of UC2825.
Could you provide the information of the RθJA, RθJC(top),RθJB.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Star,
Which package are you interested in? DIL-16 (J or N designator), SOIC-16 (DW designator) or PLCC-20 (Q or L designator).
I will check to see if the data is available.
Thanks,
Bernard
Hello
Here is the thermal data for each of the packages.
Package | Unit | |||||||
DW | PW | N | Q | FK | J | |||
RθJA | Junction-to-ambient thermal resistance | 66.4 | 91.0 | 48.6 | 54.8 | n/a | n/a | °C/W |
RθJC(top) | Junction-to-case (top) thermal resistance | 31.6 | 26.1 | 35.6 | 32.8 | 31.2 | 34.2 | °C/W |
RθJB | Junction-to-board thermal resistance | 34.1 | 42.2 | 29.6 | 19.0 | 30.9 | 48.9 | °C/W |
ψJT | Junction-to-top characterization parameter | 8.6 | 1.3 | 16.0 | 9.0 | n/a | n/a | °C/W |
ψJB | Junction-to-board thermal resistance | 33.7 | 41.6 | 29.4 | 18.7 | n/a | n/a | °C/W |
RθJC(bot) | Junction-to-ambient thermal resistance | n/a | n/a | n/a | n/a | 3.3 | 8.9 | °C/W |
Please let us know if you need any further information.
Regards
Colin