Hi,
I'm using bq27411. I found some in the forum said that bq27411 must use OTP to program some parameters before use and bq27441 doesn't need.
I have several questions:
Q1: What are the parameters that need to be programmed with OTP?
I've read the datatheet and Techenical Reference of bq27411, but didn't found those parameters.
The datasheet mentioned <SmartFlash OTP Programming(SLUA703)>, but I didn't find it on the TI web. Can somebody give me a link?
Q2:Can I use bq27411 without OTP programming? Can I write those pamameters by directly accessing the Data Memory?
It is said in the Techenical Reference:
And in the 3.1 segment, it gives a example which modifies the Desgin Capacity parameter.
Q3:The datasheet of bq27441 said:
So, bq27441 also need OTP programming? If that, what's the difference between 27411 and 27441?
Q4:Is there any program example of bq27411 on the TI web or third party web?
Thank you.
Frank