Hi,
I have followed the instructions and connected my BQ40z50EVM module with resistors to simulate the cells, powered the device with 10.6V power supply across the 1N and 4P connections, connected a 1K resistor across the pack+ and pack- pins to simulate the load. But the BQstudio software loads up and cannot detect the device. It then asks for me to select the device and BQstudio reports that it does not support the device? Any ideas why it is saying it does not support the device? I am connecting via the EV2300 comms. kit.
Also When I power the EVM module am I meant to see any LEDs lighting up? I do not see any LEDs lighting up.