According to the data sheet section 10.3.11.3 (and if I interpret it correctly):
if the POWER_ON input is tied low, the voltage at the SYS pin should go back to zero, as soon as the button is released.
I do not see this happening on the EVK. I have JP6 jumper set to low. When I power the EVK through J2, the voltage on the SYS pin appears almost immediately the PSU is turned on. The voltage stays on indefinitely and ignores the button press.
It behaves the same way, when I power the EVK through J3.
I have nothing connected to J6.
Can someone help me figure out whats going on?