Dears,
is there any SHA1 demo code can share to me?
We are using bq40z50-R1 authentication.
thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dears,
is there any SHA1 demo code can share to me?
We are using bq40z50-R1 authentication.
thanks.
Mingmo,
You can find example code for the MSP430 here. There is a lib directory in the zip package that includes C code for the SHA-1.
Todd
Todd,
thank you.
//*****************************************************************************
// MSP430F23x0 Demo - bq26100 Authentication using SHA-1 HMAC Algorithm
//
// The MSP430 performs the SHA-1 HMAC that is compatible with the bq26100.
// Once the processor is done computing the HMAC, the main() function calls
// the SDQ commands necessary to have the bq26100 perform authentication and
// compare its results with the ones of the MCU.
// The functions used to implement the SHA1 as computed by the microcontroller
// were developed following the same guidance as described in the "How to
// Implement SHA-1/HMAC Authentication for bq26100" document. It can be
// found at www.ti.com by searching for SLUA389.
//
// MSP430F23x0
// -----------------
// /|\| XIN|-
// | | |
// --|RST XOUT|-
// | |
// | P1.0|--> STATUS
// | P1.1|<-> SDQ
//
// R. Wu
// Texas Instruments Inc.
// February 2010
// Built with IAR Embedded Workbench Version: 4.21A
//*****************************************************************************
#include <stdlib.h>
#include "..\..\lib\VLO_RAND\vlo_rand.h"
#include "..\..\lib\SDQ\MSP430_SDQLIB.h"
#include "..\..\lib\SDQ\SDQ_writeByte.h"
#include "..\..\lib\SHA1_HMAC\SHA1_HMAC.h"
#define P1_STATUS BIT0
#define STATUS_FAIL (P1OUT&=~P1_STATUS)
#define STATUS_GOOD (P1OUT|=P1_STATUS)
#define STATUS_TOGGLE (P1OUT^=P1_STATUS)
#define SDQ_ERROR 0x00
extern UINT8 Message[RANDMESGNUMBYTES]; // Random message sent to the bq26100
extern UINT8 Key[SECRETKEYNUMBYTES]; // Secret key - should match bq26100
extern UINT32 Digest_32[5]; // Result of SHA1/HMAC obtained by MCU
extern UINT32 H[5];
UINT8 DeviceID[DEVICEIDNUMBYTES]; // Stores the Device ID data
UINT8 Digest[DIGESTNUMBYTES]; // SHA1 response from the bq26100
//*****************************************************************************
// void error(void)
//
// Description : Continuously blinks the status LED to denote error condition
// Returns : Nothing
//*****************************************************************************
void error(void)
{
unsigned int j;
while (1)
{
STATUS_TOGGLE;
for (j = 0; j < DEVICEIDNUMBYTES; j++)
{
SDQ_delayUSEC(8000);
}
}
}
//*****************************************************************************
// void main(void)
//
// Description : This is the main function. It calls the SDQ
// communication and the SHA1 function. Results
// is displayed through the status LED.
// Arguments : read - generic variable for read functions
// i - used for repeat loops
// Global Variables : Message[], Key[], Digest[], Digest_32[]
// Returns : Nothing
//*****************************************************************************
void main(void)
{
UINT8 read;
int i;
WDTCTL = (WDTPW | WDTHOLD); // Stop watchdog timer
P1SEL &= ~P1_STATUS; // P1.x GPIO function
P1DIR |= P1_STATUS; // P1.x STATUS output direction
STATUS_FAIL; // Initialize STATUS = FAIL
// Generate random seed to create the random message
read = (UINT8)TI_getRandomIntegerFromVLO();
srand(read);
for (i = 0; i < RANDMESGNUMBYTES; i++)
{
Message[i] = rand();
}
SHA1_authenticate(); // Perform my own SHA1 (Host side)
SDQ_init(); // Initialize SDQ comm module
// TODO: Insert the private 128-bit key that is stored in the bq26100
// Key[15..8] = K1 (highest 64 bits of the key)
// Key[ 7..0] = K0 (lowest 64 bits of the key)
// In this example 0x00000000000000000000000000000000 is used since a fresh
// unprogrammed bq26100 device should contain all 0's for its 128-bit key.
for (i = 0; i < SECRETKEYNUMBYTES; i++)
{
Key[i] = (UINT8)0x00;
}
// Read Control Register
SDQ_reset();
read = SDQ_detect();
if (read == SDQ_ERROR)
{
error();
}
SDQ_writeByte(0xCC); // Skip ROM Command
SDQ_writeByte(0x88); // Read Control Command
SDQ_writeByte(0x00); // Write Address Low Byte
SDQ_writeByte(0x00); // Write Address High Byte
read = SDQ_readByte(); // Read CRC
read = SDQ_readByte(); // Read Data to Verify Write
read = SDQ_readByte(); // Read CRC
// Read Silicon Revision Number
SDQ_reset();
read = SDQ_detect();
if (read == SDQ_ERROR)
{
error();
}
SDQ_writeByte(0xCC); // Skip ROM Command
SDQ_writeByte(0x88); // Read Control Command
SDQ_writeByte(0x01); // Write Address Low Byte
SDQ_writeByte(0x00); // Write Address High Byte
read = SDQ_readByte(); // Read CRC
read = SDQ_readByte(); // Read Data to Verify Write
read = SDQ_readByte(); // Read CRC
// See if we can read the ID of the bq26100 that should be on the SDQ bus
// Should be something like [F9 01 0F FD EB 6C 1A 89]
SDQ_reset(); // Send 160-bit Message to bq26100
SDQ_detect();
if (read == SDQ_ERROR)
{
error();
}
SDQ_writeByte(0x33); // Read ID Command
for (i = 0; i < DEVICEIDNUMBYTES; i++)
{
DeviceID[i] = SDQ_readByte(); // Read in each ID byte
}
// Write 20 bytes (160 bits) into the Message registers starting at 0x0000
SDQ_reset(); // Send 160-bit Message to bq26100
read = SDQ_detect(); // SDQ-based device connected?
if (read == SDQ_ERROR)
{
error();
}
SDQ_writeByte(0xCC); // Skip ROM Command
SDQ_writeByte(0x22); // Write Message Command
SDQ_writeByte(0x00); // Write Address Low Byte
SDQ_writeByte(0x00); // Write Address High Byte
SDQ_writeByte(Message[0]); // Write 1st byte of message
read = SDQ_readByte(); // Read CRC
// CRC not calculated by MCU; results given by the bq26100 are ignored
read = SDQ_readByte(); // Read Data to Verify Write
for (i = 1; i < RANDMESGNUMBYTES; i++) // Write remaining bytes of message
{
SDQ_writeByte(Message[i]);
read = SDQ_readByte(); // Read CRC
read = SDQ_readByte(); // Read Data
}
// Write Control to set AUTH bit to initiate Authentication by bq26100
SDQ_reset();
read = SDQ_detect();
if (read == SDQ_ERROR)
{
error();
}
SDQ_writeByte(0xCC); // Skip ROM Command
SDQ_writeByte(0x77); // Write Control Command
SDQ_writeByte(0x00); // Write Address Low Byte
SDQ_writeByte(0x00); // Write Address High Byte
SDQ_writeByte(0x01); // Write AUTH Bit of CTRL Register
read = SDQ_readByte(); // Read CRC
read = SDQ_readByte(); // Read Data to Verify Write
// Read Digest from bq26100
SDQ_reset();
read = SDQ_detect();
if (read == SDQ_ERROR)
{
error();
}
SDQ_writeByte(0xCC); // Skip ROM Command
SDQ_writeByte(0xDD); // Read Digest Command
SDQ_writeByte(0x00); // Write Address Low Byte
SDQ_writeByte(0x00); // Write Address High Byte
read = SDQ_readByte(); // Read CRC
for (i = 0; i < DIGESTNUMBYTES; i++) // Read Digest
{
Digest[i] = SDQ_readByte();
}
read = SDQ_readByte(); // Read CRC of Digest
// The 20 bytes of the digest returned by the bq26100 is arranged in 32-bit
// words so that it can be compared with the results computed by the MCU
Digest_32[4] = (UINT32)(Digest[ 0])*0x00000001 +
(UINT32)(Digest[ 1])*0x00000100 +
(UINT32)(Digest[ 2])*0x00010000 +
(UINT32)(Digest[ 3])*0x01000000;
Digest_32[3] = (UINT32)(Digest[ 4])*0x00000001 +
(UINT32)(Digest[ 5])*0x00000100 +
(UINT32)(Digest[ 6])*0x00010000 +
(UINT32)(Digest[ 7])*0x01000000;
Digest_32[2] = (UINT32)(Digest[ 8])*0x00000001 +
(UINT32)(Digest[ 9])*0x00000100 +
(UINT32)(Digest[10])*0x00010000 +
(UINT32)(Digest[11])*0x01000000;
Digest_32[1] = (UINT32)(Digest[12])*0x00000001 +
(UINT32)(Digest[13])*0x00000100 +
(UINT32)(Digest[14])*0x00010000 +
(UINT32)(Digest[15])*0x01000000;
Digest_32[0] = (UINT32)(Digest[16])*0x00000001 +
(UINT32)(Digest[17])*0x00000100 +
(UINT32)(Digest[18])*0x00010000 +
(UINT32)(Digest[19])*0x01000000;
// The results produced by the MCU and bq26100 must match for success
if ( (Digest_32[0] == H[0]) && (Digest_32[1] == H[1]) &&
(Digest_32[2] == H[2]) && (Digest_32[3] == H[3]) &&
(Digest_32[4] == H[4]) )
{
STATUS_GOOD; // Output pin status = SUCCESS
}
else
{
STATUS_FAIL; // Output pin status = FAILURE
}
}