Hello,
I'd like to know whether or not TPS40057 can tolerate higher than 3.7V on SS/SD pin as long as the voltage is lower than ABS max voltage?
I have a design where TPS40057 Shut Down signal is controlled by an open collector transistor. However, the Shut Down signal trace may see leakage from other circuitry during normal operation when power supply is ON. This leakage will charge the capacitor on SS/SD pin to more than 3.7V. Basically this is a similar situation where external voltage is driving the SS/SD pin.
Since the SS/SD pin is connected to the error amplifier I'm wondering is it safe to use TPS40057 this way and will this have a negative effect on performance?
Thanks, Tuomas