This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Looking for LED Driver

Other Parts Discussed in Thread: TLC59108
Hi all.

I am looking for LED Driver.
My customer uses it the following condition.
Vin:5V
Channels:5 (1 straight & 5 parallel)
LED current(typ): 8.5mA/ch
LED Vf: min:2.58V typ:2.8V max:3.16V
Control:PWM or I2C

Please tell me such device.

Best Regards,
Sho