This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28063 _ High-Power 15kW PFC design

Other Parts Discussed in Thread: UCC28063, UCC28070

Hi Everyone,

I am working on a 15kW battery charger. It consists of

1. AC/DC boost PFC rectifier

2. isolated Full-Bridge DC/DC stage

My question is about AC/DC boost interleaved PFC. Input: 240VAC, 1phase. Output: 700 VDC, 25A 

I plan to use UCC28063 or similar controller to drive interleaved PFC converter.

Cost is less important than development time. DSP controller is a worst case option

1. Since most sources refer to <1kW designs on those type of off-the-shelf controllers, have you been able to get it working on this power ranges?

2. Can UCC28063 / similar controllers be used at 15kW power range with 2 inteleaved phases and SiC MOSFETs ?

3. Do you feel it is better to split into 2x converters delivering 7.5kW each (with 4 phases total)?

  • By the way, input voltage range may be pretty narrow - 240 VAC 1phase +-10%.
    That should minimize the requirements for inductor and capacitors size.

    By the question still open: can off-the-shelf controllers like UCC28063 be used in 7-15 kW range?
  • Hi, Alex

    15KW is really hard for UCC28063, since UCC28063 is 2phase interleaved boundary mode PFC controller. The peak current of MOSFET, inductor and freewheel diode is very high.

    I recommend UCC28070, which is 2 phase interleaved CCM PFC controller, which can handle high power, there is 6.6kW product at customer side with UCC28070.
    For 15kW, two UCC28070 with 4 phase CCM interleaved PFC would be better solution.

    ps: do you confirm it is OK for one phase AC with 15kW? not three-phase AC?

    Regards,

  • Hi Yunsheng,

    Thank you for the answer.

    I also decided to go with 2x UCC28070 giving a total of 4 phases. Glad to know there are successful cases with similar power rating.

    By chance, Are there any reference docs on mentioned project?

    Using 240VAC 1phase is a requirement even though I realize that is unconventionally high power for a single phase. 

    Do you anticipate any crucial issues with that power rating with 1phase?

    Thanks,

    Alex

  • UCC28063 also can be used for 4phase??
  • Hi, Mason

    UCC28063 cannot be used for 4 phase PFC application, since there is no sync function of UCC28063.

    Regards,

    Yunsheng