Hi,
We are considering the use of the TPS7A4001 in an application where the junction temperature might be about 140°C. The maximum operating virtual junction temperature in the datasheet is 125°C. Howxever, the storage temperature is 150°C and moreover there is a thermal protection which is triggered for a junction temperature greater than 170°C and this thermal protection is removed below 150°C (section 7.3.3 of the datasheet). We would need clarifications regarding the use of the device over temperature. If the device is operated with a junction temperature of 140°C will it meet its specification and operate as expected although the lifetime of the part might be impacted? How come the thermal protection triggers at 170°C, 20°C higher than the maximum storage temperature?
Best regards,
JF Hasson