This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28722 WBENCH reference design disparity

Expert 1350 points

Other Parts Discussed in Thread: UCC28722, UCC28720, UCC28700, UCC28700EVM-068

I'm trying to design a flyback AC-DC supply with an output of 3.3V upto 1A. I noticed some weird behavior. If I try to get a WEBENCH design from the UCC28722 product page on the TI website it says that minimum Vout is 5V. However, if I run WEBENCH from its own page I can design a 3.3V supply. Is the UCC28722 suitable for a 3.3V supply? If yes, would the attached reference design work? I'm simply asking since I'll need to get a custom transformer made for this (even for prototyping purposes) and if this controller is not suitable it would be wasted expense for me. 

UCC28722_webench_design_3851011_38_603457300.pdf