This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq40z60 - How to determine Chemistry ID using bqStudio

Other Parts Discussed in Thread: BQSTUDIO, BQ40Z60

Hi,

I am trying to use the bq40z60Eval board and bqStudio to determine the chemistry ID of a cell which is not in the predefined database.

I need some help with the following topics:

1. How do I set-up bqStudio to record voltage, current and temperature for example every second?

2. Document SLVA725 mentions that GPC Packer, which is part of bqStudio can be used to generate all required files. However, there is no such tool, option, or button, in the bqStudio Version 1.3.52 which I am using - but it is described in the help file so I suppose it must be somewhere but cannot find it. The question is how can I find and use this tool?

3. After I get this done, what would I need to do next to get the bq40z60 finally working and showing also the correct remaining battery capacity? Currently it shows always 100% no matter if the battery is fully charged or completely discharged.

I attached my current .pp log if this is required.

Thanks,

Fred

8420.bqStudio.gg.zip

  • Hi Fred,

    1. On the registers tab, there should be a button which says "Start Log". Press this and it will record your registers (including voltage, current and temperature)

    2. I would recommend using the online GPC calculator tool:. To ID the chemistry of your battery, you just need a log of voltage, current and temperature over a charge/discharge cycle and a text file.

    3. You will likely need to perform a learning cycle once you have identified your chemID. These instructions will help you perform this: 4150.LearningCycleOverview.pdf

    Best Regards,

    Ben Lough